Adjust descriptor size and position using the Position and Size Toolbar

Use the Position and Size toolbar to quickly re-position a descriptor, entering new values or incrementally increasing or decreasing the displayed values.

The Position and Size toolbar allows you to quickly see the coordinates and size of a descriptor or selection of descriptors and change the values.

Display the Position and Size toolbar

In the Definition module, click View > Position and Size toolbar to display the Position and Size toolbar

The Position and Size toolbar will be displayed at the bottom of the Definition module by default, but you can move the toolbar by clicking the border of the toolbar and dragging it to a new placement.

Some descriptors cannot be re-sized using the Position and Size toolbar, e.g. object symbols and object texts such as object name, state/value, description, atom time stamps and/or Atoms in OPC server.

ClosedRe-position a descriptor
ClosedRe-position multiple descriptors
ClosedRe-size a descriptor
ClosedRe-size multiple descriptors

See Also

Keyboard shortcuts

Adjust descriptor position and size using the mouse or keyboard

Adjust descriptor position and size using the Property Table Viewer

Re-size a symbol descriptor