To define global function keys
- If you are not in the Global area, select Area ® Global.
- Select Area ® Edit Properties.
- Click the Function Key Assignment tab.
- Select the desired function key in the Function Keys drop-down list.
- Select the object you want the function key to operate on.
- If the function
key operates on a digital, analog, table or counter object, do the following:
- In the Index list, select the atom for which you want to change the value (only available for analog and table objects).
- In the Command/Value list, select the command (digital objects) or value you want to send to the object.
- Repeat steps 4 - 6 for each function key you want to assign.
- Click OK to save the new function key assignments.
Up to 24 function keys may be defined for each diagram.
During supervision the function keys defined as 1 - 12 are activated with
the keys F1 through F12, while the keys defined as
13 - 24 are activated with shift
+ F1 to F12.
A maximum of 15 of the 24 possible function keys may have
values attached.
24 global function keys may be defined which are
global to the entire configuration.
See Also
"To define diagram function keys"