To define diagram function keys
- Define a new diagram or open the Diagram Properties dialog box for an existing one.
- Click the Function Key Assignment tab
- Select the Enable Function Keys check box to enable this functionality.
- The name and description of the diagram is automatically displayed and cannot be changed.
- Select the desired function key in the Function Keys drop-down list.
- Select the object you want the function key to operate on.
- If the function
key operates on a digital, analog, table or counter object, do the following:
- In the Index list, select the atom for which you want to change the value (only available for analog and table objects).
- In the Command/Value list, select the command (digital objects) or value you want to send to the object.
- Repeat steps 3 - 5 for each function key you want to assign.
- Current object shows a list of function keys defined with their assigned object, index values and command/values.
- Click OK to save the new function key assignments.
Up to 24 function keys may be defined for each diagram.
During supervision the function keys defined as 1 - 12 are activated with
the keys F1 through F12, while the keys defined as
13 - 24 are activated with shift
+ F13 to F24.
A maximum of 15 of the 24 possible function keys may have
a value or a command attached per diagram.
24 global function keys may be defined which are
global to the entire project.
Note that F1 is used to access context-sensitive Help. If you assign a function to this key, it will override the access to Help
See Also