The Graph Status bar

The status bar (shown in the grey bar at the bottom of the graph) displays the status of data retrieval for signals (object atoms) when the graph is opened and being populated with data or, if a graph, when scrolling along the X-axis, changing time period.

The status bar can be removed from the graph by clearing the Display graph statusbar check box on the Options tab in the Properties form (the General tab for Embedded Graph Basic).

See Also

"Graph Properties Form", or

"XY-Plot Properties Form"