Scaling analog or table objects

Once you have defined a scaling object, you can reuse it as many times as you like to scale analog or table objects. Click How To for a step-by-step procedure.

It is recommended to define scaling objects in the Global area to make them available in all areas within the configuration.

Preconditions

Before you scale an analog or table object, the following preconditions must be met:

If the scaling object changes

If you change the properties of a scaling object, all objects that are linked to it will be affected.

See Also

The Scaling Object Properties form

To scale analog or table objects

To define a scaling object

To change scaling object properties

Example: Using a scaling object to convert Fahrenheit to Celsius