To change scaling object properties

  1. Double-click the descriptor representing the scaling object or select Edit ® Open By Name to find the object.
  2. Change the properties, as required.

images\CHICLET.gif How?

  1. Click OK to save your changes.

If the scaling object is linked to other objects, they will inherit the changes automatically.

 

See Also

What is a scaling object?

The Scaling Object Properties form

To scale analog or table objects

To define a scaling object

To change scaling object properties

Example: Using a scaling object to convert Fahrenheit to Celsius