Use the Scaling Object Properties form to:
Define a new scaling object or double-click the symbol of an existing one.
The dialog box contains the following tabs. Click on any of the tabs for further information.
For an explanation of the individual items in the dialog box, click the in the upper right hand corner of the dialog box, then click the item you want information about.
See Also
To scale analog or table objects
To change scaling object properties
Example: Using a scaling object to convert Fahrenheit to Celsius