What are Graphs?

IGSS offers the possibility of viewing statistic data in Graphs.

Graphs in IGSS display variations in object states or values with respect to time and can give a quick overview of the characteristic behavior of selected key process components.

Below is a graph showing wind speed data over a time period. Object signals on the Y-axis and time values on the X-asis:

Operators can use graphs to:

IGSS graphs are capable of combining current trends and historical data in the same chart, enabling the operator to see at a glance what happened in the process just before and immediately after an intervention or incident.

Supported object types

A graph chart can contain values or states of up to 16 signals. A signal can be an IGSS object atom. All values and states from Analog, Counter, Digital and Table object types can be displayed in a graph.

The data source can be log data, (*.log), reduced data (*.bcl), HourDayMonth data (HDM) or a combination of the data types. Live object data can also be displayed in the graph.

Graphs in IGSS are considered to be container objects (auxiliary objects) and can be referenced as objects using descriptors such as buttons, rectangles or the graph object symbol.

The IGSS Object-Level Protection feature can also be applied, helping to prevent unauthorized users from opening the graph.

Graph types

Common methods of creating graphs are:

Predefined

A predefined Graph is created in advance by the System Integrator in the Definition module, and can be edited, maintained and deleted by anyone with System Integrator user rights.

The operator can open predefined graphs in the Supervise module from the Graph menu or by clicking on a descriptor such as symbols, buttons, images and clickable areas representing the graph in a process diagram.

Properties can be edited by the operator during supervision for temporary use, but the changes to the predefined graph/XY-plot will not be saved when the project is closed. However, the operator can use a predefined graph as basis for creating an Operator Graph with the same or changed properties and save it on the operator’s own local PC. Only people with access to this PC will be able to open, edit and delete it.

There are two ways of creating (and displaying) predefined graphs:

Graphs in separate windows

Embedded Graphs

Operator created graphs

The operator can create a graph on-the-fly in the Supervise module during supervision. In the Supervise diagrams, the operator selects which IGSS objects to include in the graph and then selects Graph -> Create Graph. This function is very useful if the operator wants to monitor a specific process component before and after an intervention.

The operator graph can be saved as user-defined (*.usr) on the local work station. When re-opened, the graph will be dynamically updated. User-defined operator graphs are not displayed in the Graph menu in Supervise.

Kindly refer to the help in the IGSS Supervise module for more information on how to create and use the operator graph.

Dashboard graphs

Dashboard graphs are created and displayed in the Dashboard module, which is used to provide the operator with a quick overview of the process by combining different data representations in one view.

Dashboard graphs are simpler with much less design and navigation options than the other graph types. They can be created and maintained by both the System Integrator and the operator in the Dashboard module using the Graph widget.

For more information on how to create and navigate Dashboard Graphs, please refer to the Dashboard Help.

Example of Dashboard Graph, a typical part of a Dashboard quick overview window.

Graph menu

The Graph menu displays all available standard graphs in the active area provided that the Name to Menu or Description to menu option is selected for each graph. If the graph is displayed with a check mark in the Graph menu, the graph is open.

Graph properties

When you create a graph, you specify a number of properties using the Graph Properties form, which is identical for all types of graphs (with a few exceptions)*:

The properties of pre-defined graphs can be changed at any time by the System Integrator in IGSS Definition. User-defined Operator Graphs can be changed in IGSS Supervise.

For detailed information on how to create and navigate graphs, define properties, etc., kindly refer to the How to …. guides in the Help section.

* Embedded graph basic/Dashboard graphs used in older versions of IGSS: Available, mainly for editing of already existing graphs. This is operated differently and provides much less options.

See Also

"Graph Properties form"

"Create a new graph in a separate window"

"Create an Embedded Graph"

"Create and edit an Embedded Graph Basic"

"Graph Widget in Dashboards"

"Set graph properties as default values"