You can edit an existing object template, changing the object template properties in order to update all objects based on the template.
Some object properties are not included in object template updates. See the Changing object template properties topic.
1If the object template you want to change is not in the list of names, you have defined it in an area other than Global. Select the relevant area in the Area field to find the object template.
2 If you need to change many properties on an object template or if you need to change properties on many object templates, you can click the Property Table View button to mass-update the properties in the Property Table View form.
Define object templates in the Global area in order to make them available in all areas within the configuration.
See Also
The Property Table Viewer form
Changing object template properties
To base an object on an object template
To define a digital object template