Enable symbol resizing

If you want to re-size the symbol descriptor, you must enable symbol resizing by making the symbol scalable.

You can enable resizing for single descriptors or open the Property Table View form to enable resizing for multiple descriptors.

ClosedEnable symbol resizing (Scalable) for a single descriptor
ClosedEnable symbol re-size (scalable) for multiple descriptors

Resizing symbols for objects based on Object Templates

The Scalable check box is disabled when creating object templates. You can only make standard symbols for objects based on object templates scalable by selecting and mass-updating the object descriptors using the Property Table View form.

See Also

Re-size a symbol descriptor