Open topic with navigation
Protecting objects in Definition
Follow this step-by-step procedure when you want to protect objects
from unauthorized use.
- Identify
the objects you want to protect.
- In a new project,
mark up the objects in the data list so that you remember to protect them.
In an existing project, print the object list from the Object
Browser and mark up the objects.
- If needed,
define additional Protect objects. In most cases, the predefined Protect
object will provide enough flexibility. However, if you need more flexibility,
click
here for an example.
- Make sure
that the security level is set correctly.
Open topic with navigation