The table object properties form

From the table object properties dialog box you can:

 

How to access

Once the table object is defined and its symbol is placed on a process diagram, you can view its properties in a number of different ways.

 

The tabs

The dialog box contains the following tabs. Click on any of the tabs for further information.

images\tbl_tabs_shg.gif

 

What’s This? Help

For an explanation of the individual items in the dialog box, click the images\ico_help.gif in the upper right hand corner of the dialog box, then click the item you want information about.

See Also

Key features of a table object

Graphical display of table objects

To define a standard table object

To define a table object as a bar display

To define a table object as a moving symbol