A table object can be represented in multiple ways on a process diagram. Your choice will depend upon the nature of the object. Bar displays can be used for table objects that may contain up to ten analog objects.
Use the examples below for inspiration when deciding on which display type to choose.
The following illustrations show examples of different ways to show table objects. The symbols are taken from the default symbol file.
You can freely add your own symbols to a symbol file. All display types can be selected from the Objects menu.
To learn how to define a table object using these display forms, click the corresponding graphic.
Standard table symbol |
Rectangular field |
Bar display |
|
|
|
See Also
Key features of a table object
The table object properties form
To define a standard table object
To define a rectangular field (click-sensitive field)
To define a table object as a bar display
To define a table object as a moving symbol