Open topic with navigation
To define data management parameters
Depending on the object type,
some options will be disabled. Simply skip these steps in the procedure.
- In the Scan interval group, select the interval
defining how often the component address in the PLC is scanned.
- In the Logging group, select the percentage
with which you want process values to change before they are registered
in the log files.
- If you want
to log all data sent from IGSS to the PLC, for example, operator commands,
check the Out box.
- In the
Base interval group, select the
appropriate base interval between data
reductions.
This interval defines how often your Base
class files used for reports and graphs are updated.
- In the Data reduction group, check the boxes
of the appropriate data reduction method(s).
- This list is
grayed, if you choose None as the base interval.
- In the Transfer to history group, specify how
you want to transfer the data reduction value(s) to reports.
- You can specify
one option for each data reduction method. The method must be enabled,
before you can choose the transfer to history option.
- To include
this object in the log file printout, check the Log
to Printer box.
- To delay
alarms associated with this object, before they are registered, check
the Alarm Delay box. If you want the operator to be able to change the alarm delay period in the Object Properties form’s Data Collection & Logging tab’s Alarm delay group in the Supervise module, select the Online updateable option.
- To password-protect
this object, select the appropriate Protect
object in the Protection drop-down
list.
- To scale
this object, select the appropriate scaling object in the Scale
As drop-down list.
- To connect
this object to another object, select that object in the Connect
To drop-down list.
- If you called
this topic from a parent procedure, click here to return.
The scan intervals, logging percentages, base intervals
and alarm delay shown on this tab are defined on the Configuration tab of the System Configuration form. The System Configuration form is opened from the IGSS Master > Design and Setup tab > System Configuration button.
See Also
To define a scaling object
Open topic with navigation