Base class files hold historical data processed by the system on the basis of the seven built-in formulas (Average, Minimum, Maximum, Sum, Actual, Change and Difference).
The basis for the calculations made by the system are the data scanned in from the PLC specified by the Scan Interval on the Data Management tab of the object properties dialog box.
There are four default base intervals with which calculations may be made. The default intervals may be changed in the System Configuration program. Each base interval is called a ‘base class’ and result in a separate file.
The lowest base class (the lowest calculation interval) is called base class 2 and the highest is called base class 5
Examples of base class file names:
g2970128.bcl
g3970128.bcl
g4970128.bcl
g5970128.bcl
The second character in the file name is the base class, the ensuing six characters form the date when the files were created and the extension is an abbreviation of ‘base class’.
When all four calculation intervals are used in a configuration, there will be four files for each day.
The base class files are located in the report directory.
The base class files may be saved on the hard disk for as long as the user wishes.
Data in the base class files are used for
there are no log files for the selected object
there are no log files for the specified time period for the graph
Tips