“Auto” option for dynamically reduced scan rate
As an alternative to collecting and sending new data at the normal speed (100% spooling rate) while at the same time as transmitting the stored data (which could lead to “data congestion”) or with a scan rate significantly reduced to 1/10 (10% of normal, hence less data collected) or 1/100 (1% of normal), a new “Auto” option has been added.
Selecting the “Auto” option will reduce the spooling rate of new data dynamically at 7 pre-defined scan rates, starting with 1/1 (normal speed) the 1st hour, reducing to half speed the 2nd hour and then gradually reducing the scan rate down to 1/60 the 7th hour. In this way, more data will be collected and transferred during the retrieval of data stored during a lost connection event.
How to select the new “Auto” spooling rate