Create a link to a group diagram

You can create direct link to a group diagram, for example from a button:

  1. In the Definition module, select the Button icon.
  2. Click to place the button in the diagram you want to link from.
  3. Right-click the button and select Connect to open the Object Browser form.
  4. In the left pane of the Object Browser form, click GlobalGroup to display the group objects.
  5. In the right pane of the Object Browser form, select the group you want to connect to.
  6. Click the Open/Select button to connect to the selected group.
  7. In the Object properties form, set up the properties of the button and click the OK button to create the connection.

Only one group diagram can remain open at a time in the Supervise diagram