Use the following shortcuts to create, edit and delete objects and object templates:
For shortcut keys in blue, select the object or descriptor first
To... | Press |
---|---|
Create a rectangular field |
CTRL + 1 |
Create a command field |
CTRL + 2 |
Create a bar display |
CTRL + 3 |
Create a circular display |
CTRL + 4 |
Create a moving symbol |
CTRL + 5 |
Create an object without display |
CTRL + 6 |
Create an object template |
CTRL + SHIFT + T |
Edit object properties |
ALT + ENTER |
Delete an object |
DEL |
Find a specific object (Open by Name) |
CTRL + E1 |
Select all objects |
CTRL + A |
Connect a descriptor to an object |
CTRL + SHIFT + N |
Disconnect a descriptor from an object |
CTRL + SHIFT + S |
Lock a descriptor |
CTRL + L |
1In the Object Browser form (Ctrl+E to open): Enter F3 or CTRL+F to open the Wild card text criteria field and enter filter criteria.