Use the following shortcuts to create, open, save and install configurations:
To... | Press |
---|---|
Create a new configuration* | CTRL + N |
Open an existing configuration* | CTRL + O |
Revert to the latest saved version | CTRL + Q |
Install the configuration (stopped configuration) | CTRL + T |
Install the configuration (running configuration) | CTRL + W |
Save the configuration | CTRL + S |
* It is recommended to use the IGSS Master to create new configurations or open existing ones.