Use the following shortcuts to create, edit and manipulate areas, diagrams and graphs:
To... | Press |
---|---|
Resize descriptors when resizing a diagram | CTRL while resizing the diagram window. |
Create an area | CTRL + SHIFT + A |
Edit area properties | CTRL + F2 |
Create a diagram | CTRL + SHIFT + D |
Edit diagram properties | CTRL + F1 (active window must be a diagram) |
Set initial display | CTRL + I |
Create a graph | CTRL + SHIFT + G |
Edit graph properties | CTRL + F1 (active window must be a graph) |