To define state and command bits

  1. In the To PC box on the Bit Map I/O tab, click below the bit numbers you want to use for states. A - is inserted to indicate a state bit.
  2. In the From PC box, click below the bit numbers you want to use for commands. A - is inserted to indicate a command bit.
  3. If you want to use reverse logic, click below the appropriate bits in the Logic box.
  4. If you want to use the Single Bits option, check the appropriate boxes.