To PC (state)

Introduction

A digital object template has 32 bits which the PLC can use for states to the system.

It is completely up to the user how these 32 bits are to be used. The bits are numbered from 0 to 31.

 

Defining a state bit

To define a state bit, click below the bit to be defined to insert the - symbol.