Introduction
A digital and analog object template has 32 bits which the PLC can use for alarms to the system.
The bits are numbered from 0 to 31.
Defining an alarm bit
To define an alarm bit, click below the bit to be defined to insert one of the following symbols:
* |
|
| |
|
O |
Limit exceeded bit (Analog object templates only). |