Alarm numbers in the digital object template

If several alarm bits are set, several different alarm texts must be attached by giving different alarm numbers on the Atom Mapping tab.

When the Consecutive Alarm Numbers option is selected, you only have to type one number; the system will then automatically attach the following alarm numbers.

Consecutive alarm numbers will require you have structured your alarm texts to accommodate the consecutive alarm numbers