To define the valid commands for a given state

Valid commands can only be defined for state bits from 0-31 although subsequent bits are visible in the list.

For these state bits, a maximum of 32 valid commands can be defined.

  1. In the States list, select the state for which you want to define valid commands.
  2. In the Commands list, check the commands you want to be available when the object is in the selected state.
  3. In the Default Command drop-down list, select the default command for the selected state.
  4. Repeat steps 1 - 3 for all states.