To define alarm indication, alarm acknowledgement, alarm inhibit and limit exceeded bits

  1. In the To PC box on the Alarm In/Ack tab, do one of the following:
  1. In the From PC box, do one of the following:
  1. If you want to use the Single Bits option for alarms, check the Alarms box.
  1. In the Alarm Numbers group, choose whether you want individual or consecutive alarm numbers.