On
the Table tab, select either Fixed Table (fixed values with a fixed
number of decimals) or Float Table
(floating points represented as, for example, 7.00000e+000.
In
the Name boxes, type the exact
names of the analog objects you want to collect in the table object.
In
the Value boxes, you can optionally
type initial values for the constituent analog objects.
These
values are overwritten as soon as the data collection is started.
In
the Decimal Point box, type the
desired number of decimals.
This
option is not available for Float Table.
In
the Units box, type the appropriate
measuring unit.
In
the Minimum value box, type the
minimum value for the object.
In
the Maximum value box, type the
maximum value for the object.