To include user programs

You can add shortcuts to files of programs in the toolbar of the Supervise or Definition module in order to provide quick access to the files and programs for operators or system designers.

You can add shortcuts to executable programs, batch and com programs as well as ordinary files such as documents, text files, and spreadsheets.

If you add a link to a file that requires a special program to open, such as a .pdf file, you must ensure the program is installed on the operator machines.

ClosedTo add a short cut to a program in the toolbar of the Supervise Module
ClosedTo add a shortcut to a program in the toolbar of the Definition module

 

See Also

Including user programs