IGSS training workshops are held frequently for all user levels. Whether you are a new system integrator, an experienced SCADA developer or a programmer, you will find a workshop of interest.
All new system integrators are encouraged to attend our workshops to build up their IGSS knowledge. They will thus be able to deliver state-of-the-art SCADA projects to the end user. We see training as a very important and indispensable part of the system integrator package.
This basic 3-day workshop is for new system designers. We create a new, blank IGSS project and gradually build up a complete SCADA. More info
This 1-day workshop dives into two of the most popular external interfaces in IGSS.
ODBC can be used for configuring IGSS projects directly from a database. OPC can be used for client-side for connecting to PLC equipment through an OPC server and it can be used for server-side to allow OPC clients to get access to IGSS projects. Attendees are expected to have a good, working knowledge of IGSS. More info
Workshop Calendar
Practical Information
In case you want to use your own laptop on the workshop, please note:
You can use your own laptop during the course, but the following must be installed on your laptop at the start of the course:
- The demo version of IGSS Version 9.0 must be installed and updated.
You can download the demo version of IGSS Version 9.0 from IGSS.com. You can also install the demo version of IGSS. Version 9.0 during the course by using an IGSS installation DVD or USB keys. You can update the IGSS installation by using the IGSS Update functionality included in IGSS program.
- The Microsoft Office Suite 2007 or Microsoft Office Suite 2010 must be installed.
Customized reports (previously RMS) utilizes specific features which the Microsoft Office Suite 2007 or Microsoft Office Suite 2010 both contain. It is not possible to use earlier versions of the Microsoft Office suites as these do not contain the required features. - Microsoft SQL Server 2005 or Microsoft SQL Server 2008 must be installed.
The Audit Trail feature in IGSS requires access to a Microsoft SQL Server.
You can also install Microsoft SQL Server Express 2005 or Microsoft SQL Server Express 2008 R2 which are smaller but free versions of Microsoft SQL server.
Microsoft SQL Server Express 2005 can be downloaded from
http://www.microsoft.com/sqlserver/2005/en/us/express.aspx
Microsoft SQL Server Express 2008 R2 can be downloaded from
http://www.microsoft.com/express/Database/