PLC Driver Documentation

IGSS Comes With a Comprehensive Help System

Help as Webhelp

The IGSS help system consists of one help file for each module, plus a few thematic help files. The help files can also be viewed in a standard web browser. This provides a great advantage, because you can now search in all IGSS help files using Google or other search engines.

Documentation

For each PLC driver, the documentation includes:

  1. Software and hardware requirements.
  2. Configuring the driver in System Configuration.
  3. Configuring the objects in Definition.
  4. Performance and throughput.
  5. Error codes for troubleshooting driver alarms.