FAQ

Have a Question You Need Answered?

 
 

All Articles

Alarm log full of repeated alarm

If an object goes in and out of alarm, repeatedly, filling up the alarm log with numerous records for a specific alarm.
You might want to remove these entries from the alarm log.

This can be done using the command line tool ALMremoveNum.exe - located in the GSS folder
The commands are: ALMremoveNum folder almno 

This removes listed alarm numbers from all alarm files in the specified folder.
Several alarm numbers can be given as a space separated list.
The original files are backed up with extension *.aol.

Example: 

ALMremoveNum c:\report 1012 1013 1014 

Will remove all alarms with alarm number 1012, 1013 and 1014 from all *.alm files in the folder c:\report