FAQ

Have a Question You Need Answered?

 
 

All Articles

Jobscheduler Parameters with reports converted to version 9. Daily report Example

The report engine in version 9 is changed it was previously based on Microsoft Access. This influences the jobscheduler parameters.

You therefore need to re-configure the parameters in job scheduler.

The easiest way to proceed is to start your job scheduler from the IGSS Master module, and select Job -> Add. 

Type a name for the job and click the select button and daily report.

Change the default report name: myReportFormat to the actual report name.

Save and close, and test that your job is running as assumed

Note! For test purposes it can be an idea to change the attribute -print to -PREVIEW