FAQ

Have a Question You Need Answered?

 
 

All Articles

IGSS version 9 trying to load my version 8 configuration

If you have IGSS version 8 installed on your pc, and install a version 9 on the same pc, all version 8 registry settings will be copied to the version 9 registry in order to keep your personal settings.

This means that, on first startup, version 9 will try to open the configuration that was latest open in version 8.

If you want to run the version 9 demo configuration instead please click no to the conversion popup message and load the demo from the Open Project menu in the version 9 master.