FAQ

Have a Question You Need Answered?

 
 

All Articles

Hiding some object properties in Supervise

I don't want the plant operator to see all the tabs in the objects properties interface.

---
You can do this by setting the following parameter in the Registry:

HKEY_CURRENT_USER\Software\7-Technologies\IGSS32\V8.00.00\DefRun32_HKLM\ShowOnlyTypeSpecPages

If you set this parameter to 1, the object property interface will have a reduced number of tabs, only showing the most basic properties.

You must set this parameter manually on each of the stations where you want the reduced object property interface in Supervise.