FAQ

Have a Question You Need Answered?

 
 

All Articles

RMS report templates located on network drive

Question

I have made an RMS template and placed it in a network folder making it available on all stations in my system.

But when I run a report, I get this error:



Answer

This problem occurs because the network folder is not a trusted location in the .NET security settings.

To add your folder to the security settings, run the following command from a command prompt.
C:\WINDOWS\Microsoft.NET\Framework\v2.0.50727\caspol -q -m -ag LocalIntranet_Zone -url "\*" FullTrust -n IGSS32V8_Report
Remember to replace with the network path you're using.

Example:

C:\WINDOWS\Microsoft.NET\Framework\v2.0.50727\caspol -q -m -ag LocalIntranet_Zone -url "\\10.87.45.32\RMSTemplates\*" FullTrust -n IGSS32V8_Report