All Articles
Local Time Zone text disabling in IGSS standard reports
Question
I don't want to have the name of the local time zone displayed in the IGSS standard reports, Periodical, Snapshot and Alarm Statistics. I know that this time zone description is fetched by calling a Windows parameter. Can I disable this?
Answer
Yes, you can. However, if you disable it, then none of the standard reports will display the name of the local time zone.
To disable local time display in IGSS standard reports, go into the Windows registry and find the key:
HKEY_CURRENT_USER\Software\7-Technologies\IGSS32\7.00.00\Report_HKLM\ShowTimeZoneText
and click on ShowTimeZoneText and change the number in the Value data: box from 1 to 0. This disables the display of local time in all standard reports.