All Articles
Windows Installer 3.1 missing
Question
When running the IGSS installation, the error that the Windows Installer 3.1 is missing occurs and the installation aborts.
Answer
The Windows Installer 3.1 is not included on the CD, but can be downloaded via Windows Update or from Microsoft's website.
Download details: Windows Installer 3.1 Redistributable