FAQ

Have a Question You Need Answered?

 
 

All Articles

IGSS Update and antivirus programs

Question

Why do I get a checksum error when downloading updates via IGSS Update?

Answer

The checksum error is most likely caused by a running antivirus program. Disable the antivirus program entirely or disable checking of the [IGSS InstallPath]\gss\updates folder.

Some antivirus programs are known to prevent certain operations in IGSS. Refer to FAQ #43 - IGSS, Win XP SP2 and antivirus programs.