FAQ

Have a Question You Need Answered?

 
 

All Articles

Display or block alarms from underlying diagrams

Question

I have objects on underlying diagrams and these diagrams are referenced from buttons on the overview diagram. I need to display some of the alarms originating from objects on underlying diagrams on the overview diagram and I need to hide some of these alarms. Can I do this in some way?


Answer

Yes, it is possible to hide some of the alarms and display others. You can read the news article about Hiding alarms in IGSS here