FAQ

Have a Question You Need Answered?

 
 

All Articles

VBA-related error messages

Question

In my IGSS configuration I'm using VBA code for different purposes. Sometimes when I start either the Definition or Supervise programs, I get VBA-related error messages. Why?

Answer

Unfortunately IGSS has had some problems executing the VBA code in some configurations. This caused the VBA code to malfunction leading to VBA-related error messages.

The problem is resolved by downloading and installing the IGSS32 v4.1 Update 2 patch below.