All Articles
Transparent symbols not wanted
Question
Why are the symbols transparent on the process diagrams when my configuration is running?
Answer
Symbol masks can be shown transparently. This means that the background colour becomes visible through the symbol. Transparent is the default setting and this affects the visual appearance of the process diagram, which may confuse operators used to seeing non-transparent symbols. To change symbols to appear as non-transparent, follow the steps below.
If you do not want transparent symbol masks, do the following:
- Open the Setup program.
- On the Supervise tab, remove the check mark next to "Make symbol masks transparent".