FAQ

Have a Question You Need Answered?

 
 

All Articles

Print jobs cannot be executed by Job Scheduler

Question

I've defined a print job to be executed automatically by Job Scheduler. But when the job is due, I get an error message. Why?

Answer

If the "Run as service process" setting is enabled in the Setup program, you may get the following error message when Job Scheduler tries to execute a print job:

"Failed to render the report. Make sure you have a printer defined in your system, and sufficient memory and disk space."

The solution is to disable the "Run as service process" setting.