FAQ

Have a Question You Need Answered?

 
 

All Articles

No Help in Login and Edit Alarm Description

Question

When I call "What's This?" Help in the "Login", "Temporary Login" and the "Edit Alarm Description" dialogues, I get an error message. The access control program, AccCtrl3.dll, which controls the above dialogues calls the wrong help file in v3.0. It calls AccCtrl.hlp but should call AccCtrl3.hlp.

Answer

Download the system update attached.