FAQ

Have a Question You Need Answered?

 
 

All Articles

Missing elements in Alarm list print out

Question

I want to print the Note attached to the alarm with my Alarm list but it doesn't print. And sometimes I don't get a correct set of columns from the Alarm list on my print out. How can I remedy these problems?

Answer

The solution is an update of the ALM.EXE file, which is available in system Update 4.

Download system Update 4 and install it and the problem should be solved.