FAQ

Have a Question You Need Answered?

 
 

All Articles

Getting help on the ODBC interface

I've read that IGSS features a versatile ODBC interface, but how do I find out how to use it? The IGSS ODBC interface is described in the Interface Help file. The help file contains documentation of all the data and programming interfaces supported by IGSS.

To find the ODBC documentation, do the following:

  1. In the Igss32 3.0 Start menu, choose the Interface Help icon.
  2. On the Contents tab, open the ODBC book.