All Articles
Converting configurations older than version 8.x to IGSS32 v3
Question
What must I do to convert configurations older than version 8.x to the IGSS32 v3 format?
Answer
Detailed intructions for converting are found in the on-line help file called "Global Help". Go to the Start button on the Windows desktop, click on Programs, then IGSS32 3.0 and find and open Global Help. Click on the "Index" tab and key in as search criterium "converting". Read the instructions presented and you should be able to successfully complete a conversion.