All Articles
Can't edit objects without states
Question
Why can't I edit certain objects in IGSS WAP Services (IWS) Object List?
Answer
Due to a bug in IWS you can't edit digital objects without states or analog objects without set points. If one of these is selected, most cellular phones will show "server error" in the display. The immediate solution is to download and install the system update below.