User defined entries for command menu on diagrams and areas

If you create a visual (descriptor) in IGSS and link this to a diagram or area, you can now add user defined commands to the visual’s menu. The commands will be shown when right-clicking the reference. If you have an overview diagram showing multiple pump stations, you can provide a link on each pump station. The link could go to a map showing where the physical pump station is located.