Monitoring the IGSS Data Server

The IGSS Data Server is automatically launched when the IGSS project is started. From the IGSS Master module you can open the IGSS Data Server window. Here you can monitor the communication between the IGSS server and the operator stations.

Monitoring the IGSS Data Server communication