Events now support templates

Object Templates in Event Criteria

When defining user defined events, you can now use object templates as criteria. For example you can check if any object, based on the FLOW template, has a value higher than 50.